AXIS#.PL.FBSOURCE

Description

This parameter determines the feedback source that the position loop uses.

Value Description
0 Defers selection to AXIS#.IL.FBSOURCE - this is the default, and uses the value which is being used for commutation
1 Selects FB1 (connector X1)
2 Selects FB2 (connector X2)
3 Selects FB3 (connector X23)
4 Selects FB4 (connector X21)
5 Selects FB5 (connector X22)


  • If Axis 2 has been configured to use gantry command source (AXIS#.CMDSOURCE = 4) and the gantry is active (GANTRY.STATE = 3), if this keyword is changed, it will set the gantry state back to "pending homing" (GANTRY.STATE = 1). See GANTRY.HOME.REQUIRED documentation for more details.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 5
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
AXIS1.PL.FBSOURCE

500ch

08h

Unsigned8

-

-

Read/Write

No

AXIS2.PL.FBSOURCE

510ch

08h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.PL.FBSOURCE

5905

1711

Unsigned8

Read/Write

-

AXIS2.PL.FBSOURCE

71441

1171

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.PL.FBSOURCE

5905

Unsigned8

Read/Write

-